This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

importing legacy BIOS project

hi

i have done several projects on CCS3.3 and now i moved to CCS5.5

but i have a problem with importing these legacy project.

1st is that when i import the project a message window tells me that there are issues i need to resolve, but it doesn't show me what these errors are

2nd, when i try to open the .tcf file, it doesn't open and fives me this error:

js: "./audioapp.tcf", line 4: can't open c:/ccstud~1.1/c5500/bios/include/c55xx.cdb

js: TypeError: Cannot call method "instance" of undefined

Correct any script errors in C:/Users/aziz/workspace_v5_5/.metadata/.plugins/org.eclipse.rtsc.xdctools.buildDefinitions.DSPBIOS/.gconf/audio/audio/audioapp.tcf
using the Configuration Tool or a text editor, if necessary.


TConf initialization arguments:
-e environment['config.importPath']='C:/Users/aziz/workspace_v5_5/audio;C:/ti/bios_5_42_01_09/packages' -e environment['config.scriptName']='audioapp.tcf'

what this suppose to mean, and how can i resolve this problem without having to recreate my project from scratch?

note that i work on DSK5510