Hi,
Query 1:-
We want to know as to what is the frequency of GPMC_FCLK? Is it 100MHz or 104MHz and whether it changes to some other value during ROM boot loader? The reason is we want to compute GPMC timing parameters accurately for which we require this.
Query 2:-
We have gone through TRM AM335X, Table 7-48. GPMC Timing Parameters for Asynchronous Single Write and there we find WeOnTime = 3ns whereas the WEONTIME = 1 which means 1 GPMC_FCLK i.e. order of 10ns. Why it is so? Is it an error in the document? Again WeOffTime is shown as :- tCS + tWP + tWPH = 3ns + 25ns + 20ns. Where as Figure 7-47 in TRM, it shows WeOffTime = tCS + tWP = 20ns + 30ns. I think 3ns is wrong perhaps and rest are relative w.r.t what configuration values are chosen... please revert.
Query 3:-
How can I control these GPMC parameters when I want to flash the NOR which will hold my application code? I do not know how to do this.
Regards.