This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
As per BIOSPSP DA830 02.00.01 User Guide, after creating a CCSv4 project out of the Audio application under the examples area, I'd have to load the executable on to the DSP and plug in input and output lines appropriately as the setup. However, when i try to run the application (wtihout any sort of modification to anything else) I notice the below error:
ti.psp.mcasp.Mcasp: line 3388: E_xmtClockFail: Transmit clock failure detected
xdc.runtime.Error.raise: terminating execution
I am running the Release version of the executable (but the Debug version was faced with a similar error too). Can somebody kindly point me to what i'm missing here?
Thanks
Govind