hello,
I preparing aboard based on the AM3359 SItara processor.
I read here (https://e2e.ti.com/support/arm/sitara_arm/f/791/t/244650) that in Sep 2014 is it not recommended to boot from mmc0.
I still don't understand it. the restriction from TRM 26.1.7.5.2 says "the restriction is a reslut of many eMMC devices not being compliant with the eMMC v4.41 specification". so if I have a device compliant with eMMC v4.41 (actually 4.5) is it ok?
using MMC1 is less good for me since table 26-7 (SYSBOOT) have MMC1 only in one place. and I need the UART0 option to be before the MMC option - and there is not option for that with MMC1.
any suggestion? is there any change since Sep 2014?
P.S.
Beaglebone board uses this 4GB flash but on MMC1...