This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Jacinto 5/6 - Interrupts for SPI, how to set up?



I have a hard time understanding the interrupt handling on the Jacinto 5/6 boards.

I use the Jac 5 ref manual (SPRUGI5C) and datasheet (SPRS694B) but cannot grasp how it works.

I have gotten the SPI unit itself to work and can log the expected signals on an oscilloscope and I can communicate with EEPROM via SPI. 

Now I want some interrupts. I enable the interrupts for the SPI1 module:

#define MCSPI_IRQ_ENABLE_REG0_MASK 0xFuL
#define MCSPI_IRQ_ENABLE_REG1_MASK (0x7uL << 4uL)
#define MCSPI_IRQ_ENABLE_REG2_MASK (0x7uL << 8uL)
#define MCSPI_IRQ_ENABLE_REG3_MASK (0x7uL << 12uL)
#define MCSPI_IRQ_ENABLE_EOWKE_MASK (1uL << 17uL)

#define MCSPI_IRQ_ENABLE_MASK (MCSPI_IRQ_ENABLE_REG0_MASK | \
MCSPI_IRQ_ENABLE_REG1_MASK | \
MCSPI_IRQ_ENABLE_REG2_MASK | \
MCSPI_IRQ_ENABLE_REG3_MASK | \
MCSPI_IRQ_ENABLE_EOWKE_MASK)

In code I do:

*Spi_HwRegs[1].MCSPI_IRQENABLE = MCSPI_IRQ_ENABLE_MASK;

And before that I have installed ISR but that is the part that I am uncertain about.

Do I need to mux SPI1? How do I do that then?

What is the nbr/index of the SPI1 interrupt? I have found a little different ones and I have old code that says something that I cannot find in the datasheets at all.

SPI1 interrupt:

125 (page 236 SPRS694B datasheet)

Then the datasheet says something about "C674x DSP Interrupts" which is irrelevant I guess?

Then comes the "GP-M3 Interrupts" and then there is also "Table 7-34. External Bundle Interrupt Sources".

Which of these do I need to look at?

I want to be able user ISRs for SPI 1 to 4 (all units).