This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to boot from MMC device



hello,

i wand to connect a 4GB flash to my mmc port (either mmc0 or mmc1).

i read it should work with eMMC so i can boot from it.

in the TRM i read that for booting from emmc i need to connect only 4 data lines (1 or 4).

in the beaglebone board i see they connected the device with all 8 data lines but i'm not sure beaglebone can boot from emmc.

is anyone have 4GB emmc flash device that works?

what do you suggest for booting from emmc device - should i connect 4 line or all 8 lines?

thanks!