I am currently working with a c6746 and using AISGen v1.13 tool. It looks like this version only support COFF application file format. My questions are:
1- The Aisgen documentation states that version 1.3 supports COFF and ELF formats. Where can I find this version?
2- What are the differences in using COFF or ELF formats? (we have used only COFF format in the past).
3- Is the cfg file from v1.13 compatible with v1.3?
Thanks
Cesar