This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About DM368 DVSDK

Genius 3400 points

Other Parts Discussed in Thread: LINUXDVSDK-DV

 Hi,

      We have buy a DM368 IPNC from APPRO,but They have not supply develope SDK. And also have not find DM368 DVSDK in WIKI.

 And I want to know when DM368 DVSDK  can download.

Thanks a lot!

   

  • To start with you can use the DVSDK for DM365. At some point I think it will be updated to support DM368 (I guess mostly changes in the UBL settings for higher CLK speed, demo/codec support HD):
               http://focus.ti.com/docs/toolsw/folders/print/linuxdvsdk-dv.html
    Note that the update will probably occur on the DVSDK 3.x version.

    Even if APPRO does not provide a DVSDK you need to know under which DVSDK version (DVDSDK 2.x or DVSDK 3.x) their DM368 SW have been validated. It should be straight forward to build/run the APPRO Linux application (IPNC SW) on the DVSDK version it was validated with.

     

    Hope it helps.

    A.

  • Hi,

    I can give you the exact description of DVSDK that we are providing in IP Camera Reference Design (from Appro). Basically, we did exactly what AnBer mentioned. We have taked DVSDK 2.10.xx which was developed for DM365 and updated it with latest codecs. The UBL was created for DM368.

    TI would release DVSDK 3.x for DM365/DM368 but for this IP Camera Reference Design, current plan is not to move to this DVSDK 3.x. We would develop and productize all new features on IP Camera Reference Design on DVSDK 2.10.xx for both DM365 and DM368.

    Let me know if you want any more clarifications.

    Regards,

    Anshuman

    PS: Please mark this post as verified if you think it answers your question.

  • Thanks for your reply!

    We have download DM368IPNC software from Appro.

  • Hi

    I am using DM365  for my application.  If I wan to migrate on DM368 then what will be changes?

    Which DVSDK I should use?

    Is there more changes ?

     

    Hitesh

     

  • I also want to know the difference between DM365 and DM368 during development.  Thanks.