Hi,
I was able to install WPA-2 on my Sitara AM335x linux sdk 5.0. However, recently I downloaded the sitara linux sdk 8.0. Now, I can no longer connect to the wifi. I have tried using this
but it gives me the following error after root@am37x-evm:/usr/sbin# wpa_supplicant -d -Dnl80211 -c/etc/wpa_supplicant.conf -iwlan0 -B
wpa_supplicant v2.1-devel
random: Trying to read entropy from /dev/random
Successfully initialized wpa_supplicant
Initializing interface 'wlan0' conf '/etc/wpa_supplicant.conf' driver 'default''
Configuration file '/etc/wpa_supplicant.conf' -> '/etc/wpa_supplicant.conf'
Reading configuration file '/etc/wpa_supplicant.conf'
update_config=1
ctrl_interface='/var/run/wpa_supplicant'
eapol_version=1
ap_scan=1
fast_reauth=1
device_name='Blaze'
manufacturer='TI'
model_name='Wilink'
model_number='wl18xx'
serial_number='12345'
driver_param='use_multi_chan_concurrent=1 use_p2p_group_interface=1'
p2p_go_max_inactivity=60
p2p_go_ht40=1
disassoc_low_ack=1
concurrent_sched_scan=1
p2p_disabled=1
[ 1216.487870] cfg80211: Calling CRDA to update world regulatory domain
Could not read interface wlan0 flags: No such device
nl80211: Driver does not support authentication/association or connect commands
nl80211: Remove monitor interface: refcount=0
netlink: Operstate: linkmode=0, operstate=6
Could not read interface wlan0 flags: No such device
nl80211: Set mode ifindex 0 iftype 2 (STATION)
nl80211: Failed to set int[ 1216.666516] cfg80211: World regulatory domain upda:
erface 0 to mode 2: -19 (No such device)
wlan0:[ 1216.675859] cfg80211: DFS Master region: unset Failed to initialize de
Failed t
[ 1216.684536] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_ga)
o add interface wlan0
wlan0: Cancelling scan re[ 1216.699035] cfg80211: (2402000 KHz - 2472000 KHz )
quest
wlan0: P2P: Station mode scan operation n[ 1216.712029] cfg80211: (2457000 KH)
ot pending anymore (sta_scan_pending=0 p2p_cb_on[ 1216.725204] cfg80211: (247)
_scan_complete=0)
wlan0: Cancelling authenticat[ 1216.737988] cfg80211: (5170000 KHz - 5250000 )
ion timeout
wlan0: cancel_sched_scan called whe[ 1216.750972] cfg80211: (5735000 KHz - 58)
n no sched scan