Other Parts Discussed in Thread: SYSBIOS, AM3359
Hallo,
I'm trying to get the starterware mcspi flash example running.
When I'm running it I get the following output on the console:
[CortxA8] Exception occurred in ThreadType_Main.
Main handle: 0x0.
Main stack base: 0x83fa6530.
Main stack size: 0x1fa0.
R0 = 0x44e000e0 R8 = 0x800163b6
R1 = 0x00000000 R9 = 0x000000cd
R2 = 0x00000000 R10 = 0x00000000
R3 = 0xfffffff1 R11 = 0xffffffff
R4 = 0x8000f2d0 R12 = 0x00000000
R5 = 0x00000000 SP(R13) = 0x80010c06
R6 = 0x83ea0d58 LR(R14) = 0x83ea0e34
R7 = 0x83ea0e34 PC(R15) = 0x80010c06
PSR = 0x83ea0d58
DFSR = 0x00000005 IFSR = 0x00000000
DFAR = 0x44e000e0 IFAR = 0x00000000
ti.sysbios.family.arm.exc.Exception: line 205: E_dataAbort: pc = 0x80010c06, lr = 0x83ea0e34.
xdc.runtime.Error.raise: terminating execution
The Problem occurs when it runs the "ConsoleUtilsInit();".
If I comment all ConsoleUtil parts out, I have the same problem at "McSPI0ModuleClkConfig();" :
[CortxA8] Exception occurred in ThreadType_Main.
Main handle: 0x0.
Main stack base: 0x83fa6530.
Main stack size: 0x1fa0.
R0 = 0x00000000 R8 = 0x800158ea
R1 = 0x44e00000 R9 = 0x000000cd
R2 = 0x00000002 R10 = 0x00000000
R3 = 0xfffffff1 R11 = 0xffffffff
R4 = 0x8000e974 R12 = 0x00000000
R5 = 0x00000000 SP(R13) = 0x800158ea
R6 = 0x83ea0d58 LR(R14) = 0x83ea0e34
R7 = 0x83ea0e34 PC(R15) = 0x800158ea
PSR = 0x83ea0d58
DFSR = 0x00000805 IFSR = 0x00000000
DFAR = 0x44e00004 IFAR = 0x00000000
ti.sysbios.family.arm.exc.Exception: line 205: E_dataAbort: pc = 0x800158ea, lr = 0x83ea0e34.
xdc.runtime.Error.raise: terminating execution
I'm using the AM3359 ICE v2 with the starterware from "am335x_sysbios_ind_sdk_1.1.0.8".
Does anyones has a glue what's my mistake?
Thanks for your answers.
Tim