This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI-RTOS 2.14.00.10 UART CALLBACK ERROR



Hi,
The UART in CallBack mode still does not work. Can someone confirm?

It seems that this version of TI-RTOS continues with the issue.

Regards

Aquino

  • My recommendation is not to call UART_read() within its own callback. The driver is now buffered in the background, meaning that you can now call UART_read() to get your data as needed; without needed to setup the UART for the next read. The background buffer's size is adjustable to accommodate larger amount of data if needed.
    I've created a bug ID (SDOCM00117841) to create an example to demonstrate this.

    This "feature" was removed in 2.12 because it was labeled as a bug due to the risk that calling UART_read() within its own callback can lead to a system or task stack overflow; which can cause some real bad issues. This depended on several factors (some non-deterministic), such as the rate in which data was received, system load, system, and task stack sizes.

    Surprising, a lot of folks are requesting this to be re-enabled again so we'll provide it again in TI-RTOS 2.14.01 as "use it at your own risk". Our goal is to come up with an equation/formula that will characterize how much extra task and system stack space you will need to use this feature. As a result it will be expected that you (the user) needs to evaluate your system's worst case scenario and increase the stacks accordingly.
  • Hi Tom
    Thank you so much for your answer.
    But the CallBack think it is not working anyway.

    "My recommendation is not to call UART_read () Within its own callback"
    OK even in version 2.10_01_38 if you do the CallBack crashes.

    Really I needed an example that works. I look then waiting some example.

    Regards
    Aquino
  • Hi
    No solution?

    Regards