Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Regards.
Hi,
Important thing here would be to equalize trace lengths, because this is a parallel interface. I would say 5-10mils skew would be enough. Signal traces on Sitara boards are usually done as 50Ohm single-ended impedance lines. Impedance control is not necessary for this interface.
Slew rate is not defined. You can see section 7.7.1 of the AM335X Datasheet Rev. H for GPMC signal rise and fall times.
Hi Biser,
We are using asynchronous NOR Flash where the read and write access time is >=35ns. Still is that much length matching required? We have made the length match within +/-150mil till now..
Further will 5 inches be a long distance between AD bus between NOR Flash and ARM Controller on BBB w/o any buffer in between or shall it be ok? Actually these points have cropped after the design and layout is done.
We know that you may not see the board files but I am attaching it in case your cursory look might reveal a thing or two.
regards
MOHIT HADA said:We have made the length match within +/-150mil till now..
Yeah, I actually overdid this. 150mils should be OK. This will give 20-25ps delay between signals on longest and shortest trace. Should be no issue.
MOHIT HADA said:Further will 5 inches be a long distance between AD bus between NOR Flash and ARM Controller on BBB w/o any buffer in between or shall it be ok? Actually these points have cropped after the design and layout is done.
This should be OK without buffer.