This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 SPI BOOTMODE NOT WRKING

Dear All,

We are using the custom DM8168 design, having SPI.

We have 5 custom boards, in 2 board spi mode mode is working fine, u-boot console getting, but in remaining 3 broads SPI boot mode does not working.  

Whenever we change the SPI boot mode(10110, 4:0) and connect to JTAG through CCS application, after getting connection try to load the u-boot in SPI BOOT mode does not load while same works in the UART BOOT mode.

Our design is same in the all 5 boards, we are not getting the what is the issue, struggling since 15 days.

Please help us to resolve the issue.

Thanks,

Vidya