Hi
I've read sprueg3b.pdf and it says each core (megamodule) can be clock gated using the LPSC. If I want to power down, I use the GPSC. If I gate the clock using the LPSC and all Megamodules go to IDLE, what is the mechanism for reprogramming the LPSC to ungate the clocks?
Do I have to do this via HPI?
Can I have to host toggle an external signal that makes the LPSC ungate the megamodule clocks?
Is it possible to program the LPSC over SRIO (assuming I didn't clock gate that too)
In the documents figure "Power and Clock Domains", what is LL2?
Cheers