This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SD/MMC Card Detect Interrupt in Dm365 EVM



All,

We are adding WinCE Support for the Dm365 EVM. While adding the SD/MMC Driver, we see that the Card detect interrupt does not fire inspite of the correct CPLD configuration.

We are referring to the Register 7 in the CPLD Registers [Media Status Reg] at EMIF CE1. As anybody faced the same issue with the Card detect interrupt not firing?

Thanks,

Ravi