Other Parts Discussed in Thread: SYSBIOS
HI,
I am wrting code to send UDP to PC. I got the most of code from helloworld regarding NDK. also, I want to send UDP to PC, so I got the code from client regarding "echo UDP" command.
My existing project is using idle task to process UART data.
When I added "udpecho" to my existing project using HelloWorld project, there was no problem.
When I added code to send UDP to PC, I got the following error from CCS during runtime.
ti.sysbios.knl.Task: line 895: assertion failure: A_badPriority: An invalid task priority was used.
I googled and I fxied the problem. I put my idle task to the task with priority 2.
It meas there is no idle task provided by me. The problem was fixed.
So I want to know Can't I used idle task with NDK?
What is the reason for the above my problem?
SYS/BISO is very efficient but very frustrating because many thing is done without my knowledge.
Thanks in advance.
Baeyoung