Other Parts Discussed in Thread: TPS54620
Hello
On my EVMK2H V4 the USB port is unstable. Sometimes it works but usually it does not. When it does not work, it means that the connected device is not enumerated. Sometimes even the presence of the device is not detected. It happens no matter what kind of a device I connect. I did some investigation and I have some observations:
- we have 7 K2H EVM's, USB is working fine only on 3 of them. Some of the failed ones were just unboxed to test the USB, so nothing could have happened to them before
- on one of EVM's (maybe others too, I don't know) it seems like there is a problem with VCC5V. Even when nothing is connected to the USB port, after a few seconds from power-on the VCC5V becomes unstable and gets voltage waves reaching 6V. During these waves VCC5_PGOOD drops and 5V converter gets disabled. I have measured it on TP3 and TP4, scope screenshots available.