Hi,
I am working on IPNC RDK version 3.8 with DM8127 processor.
Current Scenario :
Right now, My own application is working with 4 H.264 Channels.
[ For that, Merge Module taking 4 inputs, give 1 output to SWOSD and then SWOSD gives to Encoder modules. ENcoder module worked with 4 input channels]
Wants to Do :
I want to do My application will work with 5 Channels (4 H.264 channels and 1 MJpeg channels).
For that, I am giving 5 input channels to Merge module and same with applied with Encoder Module.
Merge / SWOSD / Encoder has some limitation ? is there all worked with 5 Channels ?
Currently I tried to give 5 inputs to Merge....But not succeed.
Log :
host] ******************** SMART ANALYTICS USECASE WITH QUAD STREAM ********************
[host] ****** H264-1080p@30fps + H264-1080p@30fps + H264-D1@15fps + H264-D1@15fps ******
[host] 105: MCFW : CPU Revision [ES2.1] !!!
[host] 105: MCFW : Detected [UNKNOWN] Board !!!
[host] 105: MCFW : Base Board Revision [REV A] !!!
[m3vpss ] 4466: CAMERA: Create in progress !!!
[m3vpss ] Channel Num Stream 0 Ch 0 ChannelNum 0
[m3vpss ] Channel Num Stream 1 Ch 0 ChannelNum 1
[m3vpss ] 4467: CAMERA: VIP0 PortA camera mode is [ 8-bit, Non-mux Embedded Sync] !!!
[m3vpss ] 4467: CAMERA: VIP 0: VID DEC 268436737 (0x10): 0002:20202020:20202020, AUD_STATUS 538976288
[m3vpss ] Iss_captCreate:1661
[m3vpss ] !!!!!!!!!!!!!! IssAlg_capt2AInit, Entered
[m3vpss ] func: Iss_captCreate line: 1838
[m3vpss ] !!!!!!!!!!!!!! IssAlg_capt2AInit, Entered
[m3vpss ] 4472: CAMERA: Create Done !!!
[m3vpss ] 4564: CAMERA: Detect video in progress !!!
[m3vpss ] 4565: CAMERA: Detect video Done !!!
[m3vpss ] 4650: DUP : Create Done !!!
[m3vpss ] 4657: DUP : Create Done !!!
[m3vpss ] IssAlg_captTsk2A:2349: 2A task Main function Entered !!!
[m3vpss ] DCC server task running
[m3vpss ] 4661: SCLR: Create in progress !!!
[m3vpss ] 4726: SCLR : Loading Up-scaling Co-effs ...
[m3vpss ] 4727: SCLR : Co-effs Loading ... DONE !!!
[m3vpss ] SCLR:HEAPID:0 USED:64
[m3vpss ] SCLR:HEAPID:1 USED:5952
[m3vpss ] 4727: SCLR: Create Done !!!
[m3vpss ] 4728: SCLR: Create in progress !!!
[m3vpss ] 4740: SCLR : Loading Up-scaling Co-effs ...
[m3vpss ] 4740: SCLR : Co-effs Loading ... DONE !!!
[m3vpss ] SCLR:HEAPID:0 USED:64
[m3vpss ] SCLR:HEAPID:1 USED:2432
[m3vpss ] 4740: SCLR: Create Done !!!
[m3vpss ] 4741: DEI : Create in progress !!!
[m3vpss ] 4756: DEI: OUT1: 0: 0xb1b61280, 720 x 480, 4 frames
[m3vpss ] 4757: DEI : Loading Down-scaling Co-effs
[m3vpss ] 4758: DEI : Co-effs Loading ... DONE !!!
[m3vpss ] DEI:HEAPID:0 USED:64
[m3vpss ] DEI:HEAPID:1 USED:4528
[m3vpss ] 4758: DEI : Create Done !!!
[m3vpss ] 4758: DEI : Create in progress !!!
[m3vpss ] 4763: DEI: OUT0: 0: 0xb1d5b680, 320 x 192, 4 frames
[m3vpss ] 4777: DEI: OUT1: 0: 0xb1dd3680, 720 x 480, 4 frames
[m3vpss ] 4778: DEI : Loading Down-scaling Co-effs
[m3vpss ] 4778: DEI : Co-effs Loading ... DONE !!!
[m3vpss ] DEI:HEAPID:0 USED:64
[m3vpss ] DEI:HEAPID:1 USED:1008
[m3vpss ] 4779: DEI : Create Done !!!
[m3vpss ] 4779: NSF: Create in progress !!!
[m3vpss ] NSF::HEAPID:0 USED:128
[m3vpss ] NSF::HEAPID:1 USED:4928
[m3vpss ] 4785: NSF: Create Done !!!
[m3vpss ] 4787: MERGE : Create Done !!!
[m3vpss ] {SWOSD} edma3Handle->tccVal = 36
[m3vpss ] {SWOSD} edma3Handle->chId = 36
[m3vpss ] {SWOSD} edma3Handle->tccVal = 37
[m3vpss ] {SWOSD} edma3Handle->chId = 37
[m3vpss ] {SWOSD} edma3Handle->tccVal = 38
[m3vpss ] {SWOSD} edma3Handle->chId = 38
[m3vpss ] {SWOSD} edma3Handle->tccVal = 39
[m3vpss ] {SWOSD} edma3Handle->chId = 39
Regards,
Sandip Gokani