This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

K2L DDR3 configuration tool

Hi experts,

We have a custom k2l board using the same ddr(MT41K256M16RE-125IT) with that of evm. The issue is we can only run with speed  1066 but not 1333/1600 (there will be error bits if  used those rate). I guess it's because the different layouts and etch lengths. So I got questions as below: (I am using the drivers in platform libs of keystone2 pdk):

  • with the same ddr I only have to modify ddr3_phy_config  while  keeping the ddr3_emif_config as it is , right ?
  • I can  get different configurations with different rates from gel files. But I think there must be some tools used to calculate ddr configuration table. right?  Can you show me your tools which is used to configure evm-k2l so that I can make some changes to make it work with our board?

Thanks,

striker