Other Parts Discussed in Thread: TM4C129ENCPDT
Hello, here is some basic information on my setup:
Microcontroller: Tiva TM4C129ENCPDT
IDE: CCS 6.1.0.00104
SYS/Bios Version: 6.41.00.26
TI NDK Version: 2.24.00.11
I have a task that creates 6 sockets on unique port numbers and listens on these ports.
I then use fd_poll to accept incoming connections and to also receive data from them.
I can successfully accept and receive on up to 4 sockets, but when I try to connect the 5th I receive a "Connection Refused" error on my client PC.
It doesn't matter what combination of ports I connect to , it always fails on the 4th one.
It looks like fd_poll is never tripped after the first 4 connections.
I still have plenty of free heap memory according to the ROV capture below.
The NDK Stack Thread also has more than enough memory it seems.
I have set Ip.socketMaxConnections= 10.
I am still a novice when it comes to NDK, any help would be appreciated.