I am working with LCD (TFT 16 bit 565 mode ) 8080 mode. I fallowed the below link to enable lidd mode
.But i am facing the issue while u-boot is booting i am getting below isssue
U-Boot SPL 2013.10-00189-g78d8ebd-dirty (Aug 03 2015 - 13:46:03)
EVM sk boardreading args
spl: error reading image args, err - -1
reading u-boot.img
reading u-boot.img
U-Boot 2013.10-00189-g78d8ebd-dirty (Aug 03 2015 - 13:46:03)
I2C: ready
DRAM: 256 MiB
NAND: 256 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - bad CRC, using default environment
Viswa this is my NAND Image
Lcd_Init:before Setup lcd
mycode start here
data abort
MAYBE you should read doc/README.arm-unaligned-accesses
pc : [<8f76c1a0>] lr : [<8f76c190>]
sp : 8f32dea8 ip : 00000000 fp : 80614bd0
r10: 80645de2 r9 : 8f32df38 r8 : 4030cdcc
r7 : 4030cb7c r6 : 00000002 r5 : 8f793c7d r4 : 00000000
r3 : 4830e000 r2 : 00000100 r1 : 0000000a r0 : 00000013
Flags: nZCv IRQs off FIQs on Mode SVC_32
Resetting CPU ...
resetting ...
Please guide me to solve this issue .
Thanks & Regards,
pushpa teja