This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Speech codec transcoding on DSPC 8681E (continued)

Hello,

In continuation with:

My goal is just only evaluate the speech codecs. I have DSPC8681E EVM. Haven't purchased any emulator.

First thing is to simply run the codec, for ex. G.711 a-law. Input will be a wav file, output be encoded values stored in a file. That simple would be my attempt.

How can I do this simple step?

 

Second, I optimize (C language code of) the G.711 encoder, or write a transcoder myself, then I want to build and run on DSPC8681E.

How can I do this? Can I do it with just CCS? Without emulator? (FYI: DSPC8681E is connected to Host at PCI.)

How to understand the folder structure (ti.sdo.codecs.. etc etc) of codecs well?

Any video tutorials which demonstrates step-by-step about how to run these speech codecs on DSPC 8681E?

 

Useful info for your perusal:

Platform: Advantech DSPC 8681E

OS: Ubuntu 12.04, kernel 3.8.0-29

Desktop Linux SDK 1.0.3.0

BIOS MCSDK 2.1.2.6

MCSDK Video 2.2.0.45

CCSv5 (ccs_base_5.0.3.00028)

 

Thank you,

Basawaraj