This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help choosing upgrade path from C6713B

We are looking to upgrade a design which is based on a C6713B processor and will require slightly higher performance. We are comparing the C6727B and the C674x. The C6727B is attractive due to the amount of design reuse it enables (we are on a tight schedule) but we have some concerns about the product lifetime and power consumption relative to the C674x. So we have two questions:

  1. What is the projected production lifetime for the C6727B?
  2. What is the difference in power consumption between the C6727B and the C674x, assuming they are running the same process (e.g., would it consume 20% less power? etc..).

Thank you.