ARM9_0: File Loader: Verification failed: Values at address 0x00000000C3000000 do not match Please verify target memory and memory map.
ARM9_0: GEL: File: C:\Users\Jaime\Dropbox\Modem Cetrulo\evmomapl137typical\Debug\evmomapl137typical.out: a data verification error occurred, file load failed.
ARM9_0: Unable to terminate memory download: NULL buffer pointer at 0x322
I get the above error when I try to create a SYS\BIOS example. This is without any modifications. I can run rCSL arm and dsp examples, RTSC DSP Examples.
If I select OMAPL137.cmd in the build settings then I get an error that the memory map overlaps,