Hi.
I am a little confused about the Ethernet ports of AM437x. I use the AM437x IDK EVM.
As the RTM shows, AM437x should support 4 Ethernet ports--- two industrial Ethernet ports connected to PRU-ICSS1 and two gigabit Ethernet ports of the CPSW (port0 connected to A9 core). So if I want and I design the board myself and the pins don't conflict, I use these 4 ports at the same time?
And RTM section 7 table 7-11, AM437x has only two MAC addresses. Thus if I use the two industrial Ethernet ports in dual mac mode which will take two mac addresses. Then I can't use the gigabit Ethernet of CPSW because there is no mac address available. Is this understanding right ?
Thanks.
Sincerely yours,
Qinghai