Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Accessing Peripherals on I2C bus

Hi, 

we are trying set of tests simultaneously ,accessing the example code given in spectrum digital website. following tests we performed 1.LED TESTS 2.VIDEO LOOP BACK TEST 3. DDR MEMORY TESTS.. These 3 tests are given as individual examples in sample code.. we combined these codes and executed in infinite loop.. Say LED tests in infinite loop means it should run continuously, but LED blinking is stopping after some count.. 10, 12, 20,, video decoder and io expander slaves are connected via single  I2C bus. can we operate these peripherals simultaneously in infinite loop.. is it creating problem to stop LED ? suggest us solution ..

Regards,

azhagiri.s