Hi,
i'm using the following platform:
- TM4C129
- CCS : 6.1.0.00104 (it can install ARM compiler 5.1.6)
- XDCTool : xdctools_3_30_06_67_core
- ARM Compiler : 5.2.0
- TIRTOS : tirtos_tivac_2.10.01.38
and i want to use the TM4C129 as a DHCP server, so is there any ready made sample that demonstrate it?
Thanks,
Mohamed Fawzy