Hi
I am trying to use the UART ports on AM335x. I find everything works fine till baud rate 460.8Kbps. At 921.6 kbps, TX works fine but not RX.
I tried debugging the OMAP serial driver and I found that no interrupts were being received in the driver @921.6 kbps( IRQ function never gets triggered). I found the following thread
http://e2e.ti.com/support/arm/sitara_arm/f/791/p/298523/1102544
This thread suggests to use DMA and a different driver/SDK. Unfortunately our product uses SDK7. So it seems like a no fix for us. Can someone confirm what the thread conveys finally: Is the issue in AM335x hardware or is it a driver/linux limitation?
Also is there any possible thing I could try and see if it might work? Is it worthwhile to try and debug driver/kernel in case the issue lies only with the software side?
Thanks and Regards
Manbir Singh Jhawer