HI,
I have integrated 2402.4578.lcd.tar.gz LCD folder in sdk7 u-boot2013 successfully i got display image .now trying to integrate in sdk8 but i am facing some issues like below
/home/pc33702/ti-sdk-am335x-evm-08.00.00.00/board-support/u-boot-2014.07-g7e537bf/drivers/lcd/Makefile:5: /config.mk: No such file or directory
/home/pc33702/ti-sdk-am335x-evm-08.00.00.00/board-support/u-boot-2014.07-g7e537bf/drivers/lcd/Makefile:23: /rules.mk: No such file or directory
make[4]: *** No rule to make target `/rules.mk'. Stop.
make[3]: *** [drivers/lcd] Error 2
make[2]: *** [drivers] Error 2
make[1]: *** [build-one-by-one] Error 2
make: *** [sub-make] Error 2
in main 2013 u-boot main Makefile i added under this line LIBS-y += post/libpost.o my lcd path i given like this
LIBS-y += drivers/lcd/liblcd.o its got success . But in 2014 u-boot i added under libs-$(CONFIG_HAS_POST) += post/ my path is
libs-y += drivers/lcd/ this i am facing the above issue .
Also i tried like instead of adding in top directory i added in drivers make file also i change make file according to that but here i am not generating liblcd.o i am not getting display in 2014version u-boot. please guide me what are the steps we need to fallow in 2014version u-boot to add this folder successfully and display image.
Thanks & Regards,
pushpateja.c