Hello,
I'm writting a linux driver for OMAP5432 (Cortex A15) with Linux 4.0. I noticed that the cpu frequency was variable depending on the load. I need that stays fixed at the maximum frequency (2GHz).
I have disabled CPU frequency scalling, CPU idle PM and POWER_AVS option in Linux kernel but it is always variable.
Someone can help me ?