Dear TI support,
An AM335x design implements an external mux as workaround for “Multiplexed Signals GPMC_WAIT0 and GMII2_CRS Cause NAND Boot Issue” described in the errata.
As a first step the GPMC_CLK signal has been used as external Mux control IO but unfortunately this signal is driven to "low" by the rom code during the boot which makes the boot up from NAND fail
It would be then interesting then to know what pins could be used or not to drive the external mux …
So the question is what IO are driven/affected by the rom code during the AM335x boot and which could not be used as mux control signal?
Thank you
Best regards,
Guillaume