Other Parts Discussed in Thread: AM1806, DA8XX
Hello,
We are working on AM1806 processor with the BSP provided by TI . U-Boot's version is 2011.09. We have a NAND flash memory of 128Mb and 64Mb of external RAM.We need to provide field up gradability of firmware , using USB interface.
We want to understand all the possible options in U-BOOT, to upgrade firmware over USB interface –
- USB with virtual COM port (USB CDC class) ?
- USB Device Firmware Upgrade (USB DFU class) ?
- Virtual Ethernet over USB ?
Please provide further details in this regard.
Thanks and Regards,
Subrahmanyam.