Hi,
I have a problem with displaying of messages in RTA printf Logs window. Some of them can be lost sometime, as is shown on the picture:
The group of messages "To the channel..." and "Frequency is tuned..." has to display every 100 ms, but as it can be noticed some messages lost. Current log object handle - LOG_Trace2. In addition, there is LOG_Trace object handle, through of which displays a big amount of other messages, but it is disabled using LOG_disable().
OS - (DSP/BIOS 5.42.1.09)
What the problem could it be?
Thanks for reply,
Egor.