Hi,
I use sysbios_ind_sdk_2.1.0.1 and AM437x IDK EVM.
I want to use the PRU-ICSS for standard TCP/IP. The Idk 2.1 provided an example of ethernetip_adapter which is based on the TCP/IP. So I planned to reuse the ethernetip_adapter for my work. However, after analysing the code, I couldn't find how the NDK transfers the packets data to Ethernet/IP stack which is provided by Molex.
There is an function void processProtocolFrames(uint32_t* queue_number, void* userArg) in icss_eip_driver.c but it just addresses the PTP and DLR frames. I didn't find the project calling any socket related APIs.
Thanks.
Sincerely yours,
Qinghai