As shown in the picture,i use a switch chip, and its switch functions is good , but after it connects to am335x, ping function may play a role in only port ,
when i modify the cpsw_slaves[] .... phy_id = "0:00", ping function is fine only in green line , when i modify phy_id = "0:01", ping function is fine only in yellow line
and i use the switch chip in other mpu,it works ok,so I wonder the cpsw driver
so i want to konw that where is the problems and how to modify in source code to support?
I want to related guidance or the sample
thank you