This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Beaglebone Black LCD ETM0700G0BDH6

Hi there,

i got a 7'' LCD Display with Touch and want to use with BBB.(Not a Cape)

The LCD comes with 18 RGB wires and i could connnect them to the BBB.

Does the BBB recognize the LCD without having a EEPROM for the Device tree overlay? 

Do i have to build a external circuit with a EEPROM and I2C to have an ID or can i work around it on the SW?

The LCD Touchscreen has 4 wires and works with I2C with SDA,SCKL and interrupt from HOST(WAKE) and interrupt to Host(INT).

How do i activate it on BBB? I heard the Driver is already installed on Angstrom and it only needs to be activated.

But now how does this works if Yes i have to have an I2C EEPROM and I2C Touchscreen Driver simultaneously?

Regards,

Michael