Hi,
The latest ISDK(02.01.00.01) supports Ethernet/IP on AM437x PRU-ICSS.
And we were able to test the standard TCP/IP communication modifying the ethernetip_adapter example.
We want to try the same on the CPSW port instead of ICSS.
I understand that CPSW mode application is not supported in the current ISDK.
Do you have plans in future to release ethernetip_adapter example on CPSW?
Please let me know if there is any example application or example project to
test the NDK based TCP/IP communication on AM437x's CPSW.
Best Regards
Kummi