Hi,
I have a Kingston SO-DIMM (1.5V, 204pin, 8GB, 1333MHz) and I wanted to put it on the K2H EVM board. When booting it says:
U-Boot SPL 2013.01 (Apr 24 2014 - 02:06:05) SF: Detected N25Q128A with page size 64 KiB, total 16 MiB U-Boot 2013.01 (Apr 24 2014 - 02:06:05) I2C: ready Detected SO-DIMM [99U5428-065.A00LF ]
And then it stuck there.. It seems like U-boot doesn't support this dimm under current configuration. So I got 2 questions:
1. Will the DIMMs I have work on K2H EVM at all? If not I'll have to return the dimms..
2. I've cloned the source of U-boot, and there seems to be several variables related to ddr3 size or things like that.. So would you please provide any pointers to how to modify the code so that it can recognize 8GB ram?
Thanks,
Shang