Other Parts Discussed in Thread: SYSBIOS, MATHLIB
Hi,
I am trying to run a example code in dsplib using CCS6.
Looks like CCS6 did find out that there is a new package available and prompted me if that need to be installed.
I let it install DSPLIB.
Then I imported the example CCS project 'FFT_SP_Example_66_LE_ELF' successfully, but when I try to build it, it is generating some build errors.
My question is can I directly install DSPLIB latest packages to CCS6 and also can I directly import the examples as CCS project into CCS6 and be able to build them?
-Girish