This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Build root file system

I'm trying to build a custom root file system for our boards.

I'm using the ti-processor-sdk-linux-am335-evm-01.00.00.00 SDK.

I get errors when I follow the steps in processors.wiki.ti.com/.../Processor_SDK_Building_The_SDK or in arago-project.org/.../Setting_Up_Build_Environment.

ERROR: Task xxx (/home/peter/tisdk/sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/external-linaro-toolchain/external-linaro-toolchain.bb, do_install) failed with exit code '1'

How do I rebuild the minimal filesystem "arago-base-tisdk-image-am335-evm" successfully?

Is there a "menuconfig" like option so I can configure the various items included in the filesystem, and if there is how do I run it.

If there isn't, are there any instructions on how / what to modify to only include the files / busybox links that I want?

Thanks,

  Peter Steinberg