Other Parts Discussed in Thread: AM3352
Hello,
We are using a TI ARM AM3352 Processor and are having trouble with the device (gadget) USB port function. We have a custom board, very closely based on the BeagleBone Black board. When we were using the Linux/arm kernel version 3.12.9 all things were working fine. The Host and gadget portions of the USB functionality where working fine. When we upgraded the kernel to version Linux/arm 3.14.43 with the same options as in the previous working model we had, the Host USB Function still works fine, but we lose the gadget capability. The gadget we choose was the compile version of the Serial device. Are there any added options that need to select in the kernel version 3.14.43 that we need to select to get the USB gadgets working ?
Attached is our .config file (Note: Name of the file was changed to config.txt so it could be included here.)
Thank you for your time.
===============================
===============================