I am using a Beaglebone Black/Sitara processor with the HDMI output connected to a display. I am attempting to play back an HD video source of 480p and the frame update is very slow with noticeable pauses between frame updates. The OS is Linux with gstreamer-1.0 framework with standard gst plugins to decode the HD video. The example H.264 video provided with the BBB Matrix app works fine and is also a gstreamer app. However, when I switch the source to the 480p HD source the frame update is noticeably very slow.
Should I be able to playback a 480p HD video via the HDMI port with adequate frame updates? If so, would you direct me to where is that source and how to play it back?
Regards,
Jim