Hi,
It becomes MAX 1.8ns with a data sheet in rise and the fall time for input signal from NAND flash memory of AM437x and is a severe demand.
Table 5-45. GPMC and NAND Flash Timing Conditions-Asynchronous Mode
With the data sheet of NAND flash memory and AM335x of Micron, it is like 5ns.
May I determine that rise of the input signal and MAX 1.8ns of the fall time do not have any problem if satisfied between VIH=2.0V ⇔ VIL=0.8V of 3.3V specifications of AM4376?
Or is it an error in writing?
Best Regards,
Shigehiro Tsuda