Other Parts Discussed in Thread: TMS320C6424
Hello all
I successfully burn dsp image in EVM6424 NOR flash. but when i placed some sections in DDR ( in .cmd file ) the image not boot at power on ( it's booting normally when all sections placed in IRAM) . It seems that the DDR configuration is missing . could you please help me to solve this issue
I used EVM6424
my bootloader as follow
; .title "Flash bootup utility for c6424 EVM"
; .option D,T
; .length 102
; .width 140
COPY_TABLE .equ 0x42000400
;EMIF_BASE .equ 0x01E00000 ; address of EMIF registers
.sect ".boot_load"
.global _boot
_boot:
;************************************************************************
;* Debug Loop - Comment out B for Normal Operation
;************************************************************************
zero B1
_myloop: ; [!B1] B _myloop
nop 5
_myloopend: nop
;************************************************************************
;* Configure EMIF
;************************************************************************
; mvkl emif_values, a3 ; load pointer to emif values
; mvkh emif_values, a3
; mvkl EMIF_BASE, a4 ; load EMIF base address
; mvkh EMIF_BASE, a4
; mvkl 0x0024, b0 ; load number of registers to set
; mvkh 0x0000, b0
;emif_loop:
; ldw *a3++, b5 ; load register value
; sub b0,1,b0 ; decrement counter
; nop 2
; [ b0] b emif_loop
; stw b5, *a4++ ; store register value
; nop 4
;****************************************************************************
;* Copy code sections
;****************************************************************************
mvkl COPY_TABLE, a3 ; load table pointer
mvkh COPY_TABLE, a3
ldw *a3++, b1 ; Load entry point
copy_section_top:
ldw *a3++, b0 ; byte count
ldw *a3++, a4 ; ram start address
nop 3
[!b0] b copy_done ; have we copied all sections?
nop 5
copy_loop:
ldb *a3++,b5
sub b0,1,b0 ; decrement counter
[ b0] b copy_loop ; setup branch if not done
[!b0] b copy_section_top
zero a1
[!b0] and 3,a3,a1
stb b5,*a4++
[!b0] and -4,a3,a5 ; round address up to next multiple of 4
[ a1] add 4,a5,a3 ; round address up to next multiple of 4
;****************************************************************************
;* Jump to entry point
;****************************************************************************
copy_done:
b .S2 b1
nop 5