Other Parts Discussed in Thread: AM3352
Hello,
I'm a newbie dealing with AM3352 custom board and using ti-sdk-am335x-evm-07.00.00.00.
My board has
* AM3352 processor
* TPS65217C PMIC
* IS43TR16128A-125KBLI DDR3
I'm facing problem in booting using SD card. SYSBOOT[4:0] is 10111b. Created SD card using create-sdcard.sh script.
- Initially booting was getting struck in rtc32k_enable() function (Path - u-boot-2013.10-ti2013.12.01/arch/arm/cpu/armv7/am33xx/board.c). Hence commented the function call and it proceeded further.
Did changes to support TPS65217C PMIC and also DDR3 timing changes.
- Now it is getting stuck in mmc_getcd function (path - u-boot-2013.10-ti2013.12.01/drivers/mmc) at "cd = mmc->getcd(mmc);"
MMC detials :
MMC0 is used in SD/MMC connector.
MMC1 for Bluetooth-WiFi interface
MMC2 is not used
Please help me in resolving the issues.
Regards,
Lahari P.