This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM437x DDR3 Compliance test

Hi,

A compliance test of DDR3 of AM437x fails in the following items.

tCK(avg) Rising Edge Measurements

fail :2.496 ns  -0.5 % 2.500 ns <= VALUE <= 3.300 ns

Try the following:

1. Change impedance and a through rate of CK/CK# in Table 7-287.CTRL_DDR_ADDRCTRL_IOCTRL registers of TRM.
2. Exclude terminal resistance of CK/CK# and raise the reflection of the pattern on purpose.

refclk is 24MHz.

set register of the DPLL DDR is as follows: 

6.13.8.36 PRCM_CM_CLKSEL_DPLL_DDR Register (Offset = 5ACh) :0x00003202

6.13.8.37 PRCM_CM_DIV_M2_DPLL_DDR Register (Offset = 5B0h) :0x00000221
6.13.8.38 PRCM_CM_DIV_M4_DPLL_DDR Register (Offset = 5B8h) :0x00000222

What kind of thing is necessary so that tck(avg) becomes by all means than 2.5ns?

Best Regards,

Shigehiro Tsuda