This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI-Android-ICS-4.0.3-AOSP root file system compilation Error



Hi everyone i am getting some error while compiling Android 4.0 from TI source .

Help me to fix this error and go to further step.

 

Error is :

frameworks/base/include/utils/KeyedVector.h:193:31: note: declarations in dependent base ‘android::KeyedVector<android::String8, long int>’ are not found by unqualified lookup
frameworks/base/include/utils/KeyedVector.h:193:31: note: use ‘this->indexOfKey’ instead
In file included from frameworks/base/include/utils/AssetManager.h:25:0,
from frameworks/base/tools/aapt/AaptAssets.h:10,
from frameworks/base/tools/aapt/Main.h:14,
from frameworks/base/tools/aapt/Command.cpp:6:
frameworks/base/include/utils/KeyedVector.h: In instantiation of ‘const VALUE& android::DefaultKeyedVector<KEY, VALUE>::valueFor(const KEY&) const [with KEY = android::String8; VALUE = android::sp<AaptSymbols>]’:
frameworks/base/tools/aapt/AaptAssets.h:446:59: required from here
frameworks/base/include/utils/KeyedVector.h:193:31: error: ‘indexOfKey’ was not declared in this scope, and no declarations were found by argument-dependent lookup at the point of instantiation [-fpermissive]
ssize_t i = indexOfKey(key);
^
frameworks/base/include/utils/KeyedVector.h:193:31: note: declarations in dependent base ‘android::KeyedVector<android::String8, android::sp<AaptSymbols> >’ are not found by unqualified lookup
frameworks/base/include/utils/KeyedVector.h:193:31: note: use ‘this->indexOfKey’ instead
frameworks/base/include/utils/KeyedVector.h: In instantiation of ‘const VALUE& android::DefaultKeyedVector<KEY, VALUE>::valueFor(const KEY&) const [with KEY = android::String16; VALUE = unsigned int]’:
frameworks/base/tools/aapt/ResourceTable.h:485:100: required from here
frameworks/base/include/utils/KeyedVector.h:193:31: error: ‘indexOfKey’ was not declared in this scope, and no declarations were found by argument-dependent lookup at the point of instantiation [-fpermissive]
frameworks/base/include/utils/KeyedVector.h:193:31: note: declarations in dependent base ‘android::KeyedVector<android::String16, unsigned int>’ are not found by unqualified lookup
frameworks/base/include/utils/KeyedVector.h:193:31: note: use ‘this->indexOfKey’ instead
make: *** [out/host/linux-x86/obj/EXECUTABLES/aapt_intermediates/CrunchCache.o] Error 1
make: *** [out/host/linux-x86/obj/EXECUTABLES/aapt_intermediates/Command.o] Error 1
sarath-ak@sarath-ak:~/workspace/buil_android/TI-Android-ICS-4.0.3-DevKit-EVM-SK-3.0.1$ ls