Other Parts Discussed in Thread: SYSBIOS
Hi,
I have a problem with the DCAN RAM initialization on the AM437x processor. I´ve modified the procedure (appropriate registers) that works fine on the AM355x processor. In the CRTL_DCAN_RAMINIT register DCAN0_RAMINIT_START bit is set, but DCAN RAM intitialization procedure does never finish (DCAN0_RAMINIT_DONE flag is never set).
HWREG(SOC_CM_PER_REG + PRCM_CM_PER_L3S_CLKSTCTRL) =
PRCM_CM_PER_L3S_CLKSTCTRL_CLKTRCTRL_SW_WKUP;
while((HWREG(SOC_CM_PER_REG + PRCM_CM_PER_L3S_CLKSTCTRL) &
PRCM_CM_PER_L3S_CLKSTCTRL_CLKTRCTRL_MASK) != PRCM_CM_PER_L3S_CLKSTCTRL_CLKTRCTRL_SW_WKUP);
HWREG(SOC_CM_PER_REG + PRCM_CM_PER_L3_CLKSTCTRL) =
PRCM_CM_PER_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP;
while((HWREG(SOC_CM_PER_REG + PRCM_CM_PER_L3_CLKSTCTRL) &
PRCM_CM_PER_L3_CLKSTCTRL_CLKTRCTRL_MASK) != PRCM_CM_PER_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP);
HWREG(SOC_CM_PER_REG + PRCM_CM_PER_L3_INSTR_CLKCTRL) =
PRCM_CM_PER_L3_INSTR_CLKCTRL_MODULEMODE_ENABLE;
while((HWREG(SOC_CM_PER_REG + PRCM_CM_PER_L3_INSTR_CLKCTRL) &
PRCM_CM_PER_L3_INSTR_CLKCTRL_MODULEMODE_MASK) !=
PRCM_CM_PER_L3_INSTR_CLKCTRL_MODULEMODE_ENABLE);
HWREG(SOC_CM_PER_REG + PRCM_CM_PER_L3_CLKCTRL) =
PRCM_CM_PER_L3_CLKCTRL_MODULEMODE_ENABLE;
while((HWREG(SOC_CM_PER_REG + PRCM_CM_PER_L3_CLKCTRL) &
PRCM_CM_PER_L3_CLKCTRL_MODULEMODE_MASK) != PRCM_CM_PER_L3_CLKCTRL_MODULEMODE_ENABLE);
HWREG(SOC_CM_PER_REG + PRCM_CM_PER_OCPWP_L3_CLKSTCTRL) =
PRCM_CM_PER_OCPWP_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP;
while((HWREG(SOC_CM_PER_REG + PRCM_CM_PER_OCPWP_L3_CLKSTCTRL) &
PRCM_CM_PER_OCPWP_L3_CLKSTCTRL_CLKTRCTRL_MASK) !=
PRCM_CM_PER_OCPWP_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP);
HWREG(SOC_CM_PER_REG + PRCM_CM_PER_L4LS_CLKSTCTRL) =
PRCM_CM_PER_L4LS_CLKSTCTRL_CLKTRCTRL_SW_WKUP;
while((HWREG(SOC_CM_PER_REG + PRCM_CM_PER_L4LS_CLKSTCTRL) &
PRCM_CM_PER_L4LS_CLKSTCTRL_CLKTRCTRL_MASK) !=
PRCM_CM_PER_L4LS_CLKSTCTRL_CLKTRCTRL_SW_WKUP);
HWREG(SOC_CM_PER_REG + PRCM_CM_PER_L4LS_CLKCTRL) =
PRCM_CM_PER_L4LS_CLKCTRL_MODULEMODE_ENABLE;
while((HWREG(SOC_CM_PER_REG + PRCM_CM_PER_L4LS_CLKCTRL) &
PRCM_CM_PER_L4LS_CLKCTRL_MODULEMODE_MASK) != PRCM_CM_PER_L4LS_CLKCTRL_MODULEMODE_ENABLE);
HWREG(SOC_CM_PER_REG + PRCM_CM_PER_DCAN0_CLKCTRL) =
PRCM_CM_PER_DCAN0_CLKCTRL_MODULEMODE_ENABLE;
while((HWREG(SOC_CM_PER_REG + PRCM_CM_PER_DCAN0_CLKCTRL) &
PRCM_CM_PER_DCAN0_CLKCTRL_MODULEMODE_MASK) !=
PRCM_CM_PER_DCAN0_CLKCTRL_MODULEMODE_ENABLE);
while(!(HWREG(SOC_CM_PER_REG + PRCM_CM_PER_L3S_CLKSTCTRL) &
PRCM_CM_PER_L3S_CLKSTCTRL_CLKACTIVITY_GCLK_MASK));
while(!(HWREG(SOC_CM_PER_REG + PRCM_CM_PER_L3_CLKSTCTRL) &
PRCM_CM_PER_L3_CLKSTCTRL_CLKACTIVITY_GCLK_MASK));
while(!(HWREG(SOC_CM_PER_REG + PRCM_CM_PER_OCPWP_L3_CLKSTCTRL) &
PRCM_CM_PER_OCPWP_L3_CLKSTCTRL_CLKACTIVITY_GCLK_MASK ));
while(!(HWREG(SOC_CM_PER_REG + PRCM_CM_PER_L4LS_CLKSTCTRL) &
(PRCM_CM_PER_L4LS_CLKSTCTRL_CLKACTIVITY_GCLK_MASK |
PRCM_CM_PER_L4LS_CLKSTCTRL_CLKACTIVITY_CAN_CLK_MASK)));
// Start DCAN0 RAM initialization
HWREG(SOC_CONTROL_MODULE_REG + CTRL_DCAN_RAMINIT) |= CTRL_DCAN_RAMINIT_DCAN0_START_MASK;
// Wait until initialization is finished
while(!(HWREG(SOC_CONTROL_MODULE_REG + CTRL_DCAN_RAMINIT) & CTRL_DCAN_RAMINIT_DCAN0_DONE_MASK));
Do I have to set any other parameters?
Best Regards,
Slaven Dodig