Hi Forum,
I am having problem loading on demand an Ether net driver for the Micrel chip set KSZ8081 in to the kernel.
I have following setting in kernel ".config" file
CONFIG_NET_VENDOR_MICREL=y
# CONFIG_KS8842 is not set
#CONFIG_KS8851=y
#CONFIG_KS8851_MLL=y
# CONFIG_NET_VENDOR_MICROCHIP is not set
# CONFIG_NET_VENDOR_NATSEMI is not set
# CONFIG_ETHOC is not set
# CONFIG_NET_VENDOR_QUALCOMM is not set
#CONFIG_NET_VENDOR_RENESAS=y
#CONFIG_NET_VENDOR_ROCKER=y
# CONFIG_NET_VENDOR_SAMSUNG is not set
# CONFIG_NET_VENDOR_SEEQ is not set
#CONFIG_NET_VENDOR_SMSC=y
#CONFIG_SMC91X=y
# CONFIG_SMC911X is not set
#CONFIG_SMSC911X=y
# CONFIG_SMSC911X_ARCH_HOOKS is not set
# CONFIG_NET_VENDOR_STMICRO is not set
CONFIG_NET_VENDOR_TI=y
CONFIG_TI_DAVINCI_EMAC=y
CONFIG_TI_DAVINCI_MDIO=y
CONFIG_TI_DAVINCI_CPDMA=y
CONFIG_TI_CPSW_PHY_SEL=y
CONFIG_TI_CPSW_ALE=y
CONFIG_TI_CPSW=y
# CONFIG_TI_CPTS is not set
# CONFIG_NET_VENDOR_VIA is not set
# CONFIG_NET_VENDOR_WIZNET is not set
CONFIG_PHYLIB=y
CONFIG_MICREL_KSZ8081=y # ENABLE / DISABLE of these constant in the .config give
CONFIG_MICREL_KSZ8091=y # Network driver load on demand basis. or auto load basis
CURRENTLY am335x-boneblack.dtb contents... only ether net section...as follow:
ethernet@4a100000 {
compatible = "ti,cpsw";
ti,hwmods = "cpgmac0";
clocks = <0x35 0x36>;
clock-names = "fck", "cpts";
cpdma_channels = <0x8>;
ale_entries = <0x400>;
bd_ram_size = <0x2000>;
no_bd_ram = <0x0>;
rx_descs = <0x40>;
mac_control = <0x20>;
slaves = <0x2>;
active_slave = <0x1>;
cpts_clock_mult = <0x80000000>;
cpts_clock_shift = <0x1d>;
reg = <0x4a100000 0x800 0x4a101200 0x100>;
#address-cells = <0x1>;
#size-cells = <0x1>;
interrupt-parent = <0x1>;
interrupts = <0x28 0x29 0x2a 0x2b>;
ranges;
syscon = <0x2f>;
status = "okay";
pinctrl-names = "default", "sleep";
pinctrl-0 = <0x37>;
pinctrl-1 = <0x38>;
mdio@4a101000 {
compatible = "ti,davinci_mdio";
#address-cells = <0x1>;
#size-cells = <0x0>;
ti,hwmods = "davinci_mdio";
bus_freq = <0xf4240>;
reg = <0x4a101000 0x100>;
status = "okay";
pinctrl-names = "default", "sleep";
pinctrl-0 = <0x39>;
pinctrl-1 = <0x3a>;
linux,phandle = <0x3b>;
phandle = <0x3b>;
};
slave@4a100200 {
mac-address = [00 00 00 00 00 00];
phy_id = <0x3b 0x0>;
phy-mode = "rmii";
};
slave@4a100300 {
mac-address = [00 00 00 00 00 00];
phy_id = <0x3b 0x3>; <-----------------------------Modification implemented here.
phy-mode = "rmii";
};
cpsw-phy-sel@44e10650 {
compatible = "ti,am3352-cpsw-phy-sel";
reg = <0x44e10650 0x4>;
reg-names = "rmii-sel";
rmii-ref;
};
};
KERNEL LOG
[ 2.305710] mousedev: PS/2 mouse device common for all mice
[ 2.311656] i2c /dev entries driver
[ 2.320080] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 2.405224] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.415065] oprofile: using arm/armv7
[ 2.420999] Initializing XFRM netlink socket
[ 2.426160] NET: Registered protocol family 17
[ 2.431077] NET: Registered protocol family 15
[ 2.436877] Key type dns_resolver registered
[ 2.441882] omap_voltage_late_init: Voltage driver support not added
[ 2.448763] sr_dev_init: No voltage domain specified for smartreflex0. Cannot initialize
[ 2.457374] sr_dev_init: No voltage domain specified for smartreflex1. Cannot initialize
[ 2.469023] ThumbEE CPU extension supported.
[ 2.473635] Registering SWP/SWPB emulation handler
[ 2.478916] SmartReflex Class3 initialized
[ 2.502332] mmc0: host does not support reading read-only switch, assuming write-enable
[ 2.524233] mmc0: new high speed SDHC card at address b368
[ 2.546816] mmcblk0: mmc0:b368 USD 3.71 GiB
[ 2.562923] mmcblk0: p1 p2
[ 2.574196] tps65217 0-0024: Read from reg 0x16 failed
[ 2.579655] vdds_dpr: failed to enable
[ 2.592625] tps65217 0-0024: failed to register tps65217-pmic regulator
[ 2.600007] tps65217-pmic: probe of tps65217-pmic failed with error -121
[ 2.619569] tps65217 0-0024: Failed to read revision register: -121
[ 2.628282] tps65217: probe of 0-0024 failed with error -121
[ 2.636028] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 2.658698] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 100 kHz
[ 2.744139] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 2.750608] davinci_mdio 4a101000.mdio: detected phy mask fffffff6
[ 2.771034] libphy: 4a101000.mdio: probed
[ 2.775601] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver unknown
[ 2.784144] davinci_mdio 4a101000.mdio: phy[3]: device 4a101000.mdio:03, driver unknown
[ 2.795638] cpsw-phy-sel 44e10650.cpsw-phy-sel: invalid resource
[ 2.802240] cpsw-phy-sel: probe of 44e10650.cpsw-phy-sel failed with error -22
[ 2.810875] cpsw 4a100000.ethernet: Detected MACID = 68:c9:0b:7c:e1:a1
[ 2.826378] hctosys: unable to open rtc device (rtc0)
[ 2.831761] sr_init: No PMIC hook to init smartreflex
[ 2.837949] sr_init: platform driver register failed for SR
[ 2.954203] EXT4-fs (mmcblk0p2): mounted filesystem without journal. Opts: (null)
[ 2.962613] VFS: Mounted root (ext4 filesystem) readonly on device 179:2.
[ 2.989835] devtmpfs: mounted
[ 2.995773] Freeing unused kernel memory: 432K (c0846000 - c08b2000)
[ 3.343312] EXT4-fs (mmcblk0p2): warning: mounting unchecked fs, running e2fsck is recommended
[ 3.362660] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
Starting logging: OK
Initializing random number generator... [ 4.011504] random: dd urandom read with 11 bits of entropy available
done.
Starting network...
/etc/init.d/S93-am335x-pm-firmware-load: line 4: can't create /sys/devices/ocp.2/44d00000.wkup_m3/firmware/am335x-pm-firmware.bin/loading: nonexistent y
/etc/init.d/S93-am335x-pm-firmware-load: line 5: can't create /sys/devices/ocp.2/44d00000.wkup_m3/firmware/am335x-pm-firmware.bin/data: nonexistent diry
/etc/init.d/S93-am335x-pm-firmware-load: line 6: can't create /sys/devices/ocp.2/44d00000.wkup_m3/firmware/am335x-pm-firmware.bin/loading: nonexistent y
gwcs1x login: [ 8.432265] EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:758: group 16, block bitmap and bg descriptor inconsistent: 32251s
[ 8.505515] EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:758: group 17, block bitmap and bg descriptor inconsistent: 31328 vs 31124 frees
ETHER NET DRIVER KSZ8081 DRIVER CRASH
=====================================
gwcs1x login: root
# insmod ksz8081.ko # on demand basis
# ifconfig eth0 192.168.1.12 up
[ 54.859759] net eth0: initializing cpsw version 1.12 (0)
[ 54.944608] net eth0: phy found : id is : 0x221560
[ 54.950098] Unable to handle kernel NULL pointer dereference at virtual address 00000084
[ 54.958847] pgd = de530000
[ 54.961722] [00000084] *pgd=9e50b831, *pte=00000000, *ppte=00000000
[ 54.968509] Internal error: Oops: 17 [#1] SMP ARM
[ 54.973477] Modules linked in: ksz8081(O)
[ 54.977762] CPU: 0 PID: 79 Comm: ifconfig Tainted: G O 4.2.0-rc6-gec3fe91-dirty #2
[ 54.986924] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 54.993342] task: de4e3140 ti: de490000 task.ti: de490000
[ 54.999068] PC is at cpsw_phy_sel+0x3c/0x70
[ 55.003501] LR is at bus_find_device+0x78/0x8c
[ 55.008195] pc : [<c0486380>] lr : [<c03e0828>] psr: 600d0013
[ 55.008195] sp : de491dc0 ip : de4e3160 fp : 00000000
[ 55.020264] r10: 00000000 r9 : de511740 r8 : 00000000
[ 55.025770] r7 : de425600 r6 : 00000006 r5 : 00000000 r4 : de14b410
[ 55.032646] r3 : 3f6baba8 r2 : 00000000 r1 : 00000006 r0 : 00000000
[ 55.039533] Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
[ 55.047040] Control: 10c5387d Table: 9e530019 DAC: 00000015
[ 55.053094] Process ifconfig (pid: 79, stack limit = 0xde490218)
[ 55.059419] Stack: (0xde491dc0 to 0xde492000)
[ 55.064027] 1dc0: de425000 00000002 de4772f4 c0489290 00000000 00000003 00000000 c05a55a8
[ 55.072645] 1de0: 00000000 00000000 c05a5488 c0089afc 00000000 c095ffdc c095a4ac fffffff8
[ 55.081268] 1e00: 00000000 00000000 de491e4c de511740 0000000d c005ec78 ffffffff de425000
[ 55.089882] 1e20: 00001043 c063d6e0 00001002 00000000 00000000 c005ecd4 00000000 de425000
[ 55.098502] 1e40: 00000000 c063d6e0 de425030 00000000 00000000 c04fea5c c04fe9c0 de425000
[ 55.107117] 1e60: 00001043 00000001 00001002 c04feccc de425000 00000140 00001002 00000000
[ 55.115745] 1e80: 00000000 c04fedb0 de511740 de471a0c bea71ba0 00000000 00008914 c056bb68
[ 55.124365] 1ea0: 00000020 de471a00 de471a0c de425000 30687465 00000000 00000000 00000000
[ 55.132987] 1ec0: 00001043 0c01a8c0 00000001 00000000 00000000 00008914 ddab4040 bea71ba0
[ 55.141611] 1ee0: c0959340 00008914 de490000 ddab4060 bea71ba0 c04dfb88 c04dfb18 c0175ec8
[ 55.150228] 1f00: de0322c0 00000003 bea71ba0 c017582c c0065464 de186018 de4e3140 de4e3140
[ 55.158849] 1f20: dfa1c590 00000000 de4ad800 c0967d48 dfa1c580 de184ec0 de491f8c c05e76f4
[ 55.167460] 1f40: de4d0d98 c01439fc 00100073 00000000 00000000 c05e7d88 00000000 00000000
[ 55.176072] 1f60: c5bd2670 de0322c0 de0322c0 00000000 bea71ba0 00008914 de490000 00000003
[ 55.184689] 1f80: 000be008 c0175ec8 0009e39a 0009e39a bea71ba0 bea71d8c 00000036 c000f7c4
[ 55.193311] 1fa0: 00000000 c000f5e0 0009e39a bea71ba0 00000003 00008914 bea71ba0 0009e39a
[ 55.201929] 1fc0: 0009e39a bea71ba0 bea71d8c 00000036 0008b5a8 00000003 bea71eaa 000be008
[ 55.210544] 1fe0: 000bb2d8 bea71b3c 00017c7c b6eedc26 200d0030 00000003 b7df5ffe 533f7fff
[ 55.219186] [<c0486380>] (cpsw_phy_sel) from [<c0489290>] (cpsw_ndo_open+0x9c/0x608)
[ 55.227362] [<c0489290>] (cpsw_ndo_open) from [<c04fea5c>] (__dev_open+0x9c/0x104)
[ 55.235347] [<c04fea5c>] (__dev_open) from [<c04feccc>] (__dev_change_flags+0x88/0x14c)
[ 55.243786] [<c04feccc>] (__dev_change_flags) from [<c04fedb0>] (dev_change_flags+0x18/0x48)
[ 55.252695] [<c04fedb0>] (dev_change_flags) from [<c056bb68>] (devinet_ioctl+0x67c/0x774)
[ 55.261327] [<c056bb68>] (devinet_ioctl) from [<c04dfb88>] (sock_ioctl+0x70/0x2cc)
[ 55.269319] [<c04dfb88>] (sock_ioctl) from [<c017582c>] (do_vfs_ioctl+0x78/0x6b0)
[ 55.277215] [<c017582c>] (do_vfs_ioctl) from [<c0175ec8>] (SyS_ioctl+0x64/0x74)
[ 55.284939] [<c0175ec8>] (SyS_ioctl) from [<c000f5e0>] (ret_fast_syscall+0x0/0x54)
[ 55.292926] Code: e59f0034 ebfd690d e1a01006 e1a02005 (e5903084)
[ 55.299543] ---[ end trace 172496384e6a3643 ]---
Segmentation fault
# [ 170.943936] random: nonblocking pool is initialized
[ 303.843925] EXT4-fs (mmcblk0p2): error count since last fsck: 273
[ 303.850385] EXT4-fs (mmcblk0p2): initial error at time 3: ext4_mb_generate_buddy:758
[ 303.858564] EXT4-fs (mmcblk0p2): last error at time 8: ext4_mb_generate_buddy:758
I will be grateful if you please give your valuable observation advise.
Thank you,
IK