This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BBB based custom board kernel panic with 47pF on LCD lines

Other Parts Discussed in Thread: AM3354

Our company developed a custom board for a measuring device, with main function as GUI with display and ctouch.
As base schematics were used the available Altium project of the BBB + and some parts of the Chipsee 7" cape. The unused peripherals, such as ETHERNET, HDMI, ID E2PROM, CAN, ecc was removed in our project. MCU is AM3354.
We have some hw issues on this board, mainly seems that the LCD data and control lines has influence on the stability, especially on the DDR3 memory.
1. if we leave the 47pF capacitors on the LCD lines, the kernel goes always in panic
2. without those capacitors, the board is more stable
3. we are checking the RAM stability with "memtester" utility from Charles Cazabon, and we noted that if there is activity to the TFT, sometimes the test runs with errors (no 47pF capacitors)
4. our application has a display screen saver function, and when the display goes in power save, no activity on the LCD lines, the memtester runs without error (no 47pF capacitors)
The power lines to MCU and DDR3 are stable, good decoupling a buffer capacitors are present. PCB is 6 layer, DDR connections are almost idetical as on BBB, layers organization as on BBB.
Anybody has some tip, what we can check to fix this issue?
Thanks in advance, Zoli